Input Mode 3: Stop Output, Execute Opposite Compare Cycle while Fault Active

An input Event in Input mode 3 will stop the output signal and start executing the opposite dead time and on time, as long as the fault/input is active. When the input is released, the ongoing dead time and/or on time will finish and then, the normal flow will start.

If Input mode 3 is used on input A, an event will only have an effect if the TCD is in Dead-time A or On time A.
Figure 23-14. Input Mode 3 on Input A

If Input mode 3 is used on input B, an event will only have an effect if the TCD is in Dead-time B or On time B.

Figure 23-15. Input Mode 3 on Input B