Input Mode 4: Stop all Outputs, Maintain Frequency
When Input mode 4 is used, both input A and input B will give the same functionality.
An input event will deactivate the outputs as long as the event is active. The TCD counter will not be affected by events in this Input mode.