6.1.9.40.1 Abs Flag
The abs psect flag defines the current psect as being
absolute; i.e., it is to start at location 0. This does not mean that this module’s
contribution to the psect will start at 0, since other modules can contribute to the same
psect (See also Ovrld Flag).
An abs-flagged psect is not relocatable and an error will
result if a linker option is issued that attempts to place such a psect at any
location.