6.1.9.40.10 Merge Flag
This flag is deprecated. Consider, instead, using the
optim psect flag.
The merge psect flag controls how the psect will be
merged with others. This flag can be assigned 0, 1, or not specified. When assigned 0, the
psect will never be merged by the assembly optimizer during optimizations. If assigned the
value 1, the psect can be merged if other psect attributes allow it and the optimizer can
see an advantage in doing so. If this flag is not specified, then merging will not take
place.
Typically, merging is only performed on code-based psects
(text psects).