4.6.6.12 Zeroallram Option
The -fzeroallram=off|on|auto option controls which regions of data memory are
cleared by the runtime startup code. This feature is only available for Enhanced Mid-range and
PIC18 devices.
As required by the C standard, uninitialized objects with permanent storage duration must be
zeroed before main() executes. Most 8-bit PIC devices have RAM divided into
multiple data banks, and uninitialized objects could be located in many of these banks.
Adjusting how these memory regions are cleared can lead to code size savings, which is the
purpose of this option. Note, however, that this option cannot be used to disable the clearing
of uninitialized objects altogether. Use the -Wl,--no-data-init option for
that purpose.
When the option -fzeroallram=off has been issued, the compiler will generate
start up code that clears only the memory occupied by the uninitialised objects. This might
require the use of several loops to complete this task if the objects are present in more than
one data bank; however, the startup code will run fast.
When the argument to the -fzeroallram is specified as on
and the optimization level is set at -O3 or -Os, the
compiler will instead zero the entire amount of RAM present on the target device, regardless
of where the uninitialised objects have been allocated. The code to perform this will be
typically smaller than that required to clear discrete ranges; however, it might take longer
to execute. Use this feature with caution if your project contains
__persistent variables, as these are often assumed to hold their value over
a reset. An advisory message will be issued if __persistent variables are
present when this feature has been enabled. A message will also be issued if you attempt to
enable this feature when the optimization level is set to below -O3. You
might choose to enable this optimization for functional safety reasons or to assist with
debugging.
auto, the compiler will zero the
entirety of data memory only if it results in smaller code and the following are true.- Level
-Osoptimizations have been selected - There are no objects qualified
__persistant - There are no assembly modules and there are no variables defined in inline assembly
- The
-mramoption has not been used to modify the default RAM configuration in any way - Neither the
-mcodeoffsetnor-mmaxichipoption have been used