5.9.2.2.1 Monitor Security Network NAS Switch
The Network Access Server Switch Status page provides an overview of the current NAS port states.

The Network Access Server Switch Status page has the following parameters:
- Port: The switch port number. Click to navigate to detailed NAS statistics for this port.
- Admin State: The port's current administrative state. See NAS Admin State for a description of possible values.
- Port State: The current state of the port. See NAS Port State for a description of the individual states.
- Last Source: The source MAC address carried in the most recently received EAPOL frame for EAPOL-based authentication, and the most recently received frame from a new client for MAC-based authentication.
- Last ID: The username (supplicant identity) carried in the most recently received Response Identity EAPOL frame for EAPOL-based authentication, and the source MAC address from the most recently received frame from a new client for MAC-based authentication.
- QoS Class: QoS Class assigned to the port by the RADIUS server if enabled.
- Port VLAN ID: The VLAN ID that NAS has put the port in. The field is blank if the Port VLAN ID is not overridden by NAS. If the VLAN ID is assigned by the RADIUS server, RADIUS-assigned is appended to the VLAN ID. If the port is moved to the Guest VLAN, Guest is appended to the VLAN ID.