5.9.2.2.2 Monitor Security Network NAS Port
The NAS Statistics page provides detailed NAS statistics for a specific switch port running EAPOL-based IEEE 802.1X authentication. For MAC-based ports, it shows selected backend server (RADIUS Authentication Server) statistics, only.

The NAS Statistics page has the following parameters:
- Port State
- Admin State: The port's current administrative state. Refer to NAS Admin State for a description of possible values.
- Port State: The current state of the port. Refer to NAS Port State for a description of the individual states.
- QoS: The QoS class assigned by the RADIUS server. The field is blank if no QoS class is assigned.
- Port VLAN ID: The VLAN ID that NAS has put the port in. The field is blank if the Port VLAN ID is not overridden by NAS. If the VLAN ID is assigned by the RADIUS server, RADIUS-assigned is appended to the VLAN ID. If the port is moved to the Guest VLAN, Guest is appended to the VLAN ID.
- Port Counters
- EAPOL Counters:
These supplicant frame counters are available for the following
administrative states:
- Force Authorized
- Force Unauthorized
- Port-based 802.1X
- Single 802.1X
- Multi 802.1X
Figure 5-27. EAPOL Counters 
- Backend Server
Counters: This backend (RADIUS) frame counters are available for
the following administrative states:
- Port-based 802.1X
- Single 802.1X
- Multi 802.1X
- MAC-based
Auth.
Figure 5-28. Backend Server Counters 
- Last Supplicant/Client
Information: Information about the last supplicant/client that
attempted to authenticate. This information is available for the
following administrative states:
- Port-based 802.1X
- Single 802.1X
- Multi 802.1X
- MAC-based
Auth.
Figure 5-29. Last Supplicant/Client Information 
- EAPOL Counters:
These supplicant frame counters are available for the following
administrative states:
- Selected Counters: The
Selected Counters table is visible when the port is in one of the following
administrative states:
- Multi 802.1X
- MAC-based
Auth.
The table is identical to and is placed next to the Port Counters table. It is empty if no MAC address is currently selected.
- Attached MAC Addresses
- Identity: Shows the identity of the supplicant, as received in the Response Identity EAPOL frame. Clicking the link causes the supplicant's EAPOL and Backend Server counters to be shown in the Selected Counters table. If no supplicants are attached, it shows No supplicants attached. This column is not available for MAC-based Auth.
- MAC Address: For Multi 802.1X, this column holds the MAC address of the attached supplicant. For MAC-based Auth., this column holds the MAC address of the attached client. Clicking the link causes the client's Backend Server counters to be shown in the Selected Counters table. If no clients are attached, it shows No clients attached.
- VLAN ID: This column holds the VLAN ID that the corresponding client is currently secured through the Port Security module
- State: The client can either be authenticated or unauthenticated. In the authenticated state, it is allowed to forward frames on the port, and in the unauthenticated state, it is blocked. If the backend server hasn't successfully authenticated the client, it is unauthenticated. If an authentication fails for one or the other reason, the client remains in the unauthenticated state for Hold Time seconds.
- Last Authentication: Shows the date and time of the last authentication of the client (successful and unsuccessful)