4.11.2 Aggregation Groups Configuration
The Aggregation Group Configuration page is used to configure the aggregation groups.
The Aggregation Group Configuration page has the following parameters:
- Group ID: Indicates the aggregation group ID for the settings contained in the same row. Group ID Normal indicates there is no aggregation. Only one group ID is valid per port.
- Port Members: Each switch port is listed for each group ID. Select a radio button to include a port in an aggregation or clear the radio button to remove the port from the aggregation. By default, no ports belong to any aggregation group. Only full duplex ports can join an aggregation and ports must be at the same speed in each group.
- Mode: This parameter
determines the mode for the aggregation group.
- Disabled: The group is disabled
- Static: The group operates in static aggregation mode
- LACP (Active): The group operates in LACP active aggregation mode. See IEEE 801.AX-2014, section 6.4.1 for details.
- LACL (Passive): The group operates in LACP passive aggregation mode. See IEEE 801.AX-2014, section 6.4.1 for details.
- Revertive: This parameter only applies to LACP-enabled groups. It determines if the group performs automatic link (re-)calculation when links with higher priority become available.
- Max Bundle: This parameter only applies to LACP-enabled groups. It determines the maximum number of active bundled LACP ports allowed in an aggregation.