4.10.1.6 Security Switch Access Management Configuration
Configure the Access Management table on the Access Management Configuration page, as shown in the following figure. The maximum number of entries is 16. If the application's type matches any one of the access management entries, then it allows access to the switch.
The Access Management Configuration page has the following parameters:
- Mode: Indicates the access
management mode operation. Possible modes are:
- Enabled: Enable access management mode operation
- Disabled: Disable access management mode operation
- Delete: Check to delete the entry. It is deleted during the next save.
- VLAN ID: Indicates the VLAN ID for the access management entry
- Start IP Address: Indicates the end IP unicast address for the access management entry
- End IP Address: Indicates the end IP unicast address for the access management entry
- HTTP/HTTPS: Indicates that the host can access the switch from HTTP/HTTPS interface, if the host IP address matches the IP address range provided in the entry
- SNMP: Indicates that the host can access the switch from SNMP interface, if the host IP address matches the IP address range provided in the entry
- Telnet/SSH: Indicates that the host can access the switch from TELNET/SSH interface, if the host IP address matches the IP address range provided in the entry