4.1.6 System Log Configuration
Configure the Syslog server IP address and Syslog Level severity, as shown in the following figure.

The System Log Configuration page has the following parameters:
- Server Mode: Indicates the server mode
operation. The syslog protocol is based on UDP
communication and received on UDP port 514, and
the syslog server does not send acknowledgments to
sender, as UDP is a connectionless protocol, and
it does not provide acknowledgments. The syslog
packet always sends out even if the Syslog server
does not exist. The following are the possible
modes:
- Enabled: Enables server mode operation
- Disabled: Disables server mode operation
- Server Address: Indicates the IPv4 host address of syslog server. If the switch provides DNS feature, then it can also be a domain name.
- Syslog Level: Indicates the kind of
message that is sent to the syslog server. The
following are the possible modes:
- Error: Send specific messages regarding the severity code that is less than or equal to Error (3)
- Warning: Send specific messages regarding the severity code that is less than or equal to Warning (4)
- Notice: Send specific messages regarding the severity code that is less than or equal to Notice (5)
- Informational: Send specific messages regarding the severity code that is less than or equal to Informational (6)