4.18.10 QoS Control List Configuration
The QoS Control List Configuration page shows the QoS Control List (QCL), which is made up of the QCEs. Each row describes a QCE that is defined. The maximum number of QCEs is 256 on each switch.
Click the plus icon to add a new QCE to the list.


The QoS Control List Configuration page has the following parameters:
- QCE: Indicates the QCE id
- Port: Indicates the list of ports configured with the QCE or Any
- DMAC: Indicates the destination MAC address. Possible values are:
- Any: Match any DMAC
- Unicast: Match unicast DMAC
- Multicast: Match multicast DMAC
- Broadcast: Match broadcast DMAC
- <MAC>: Match specific DMAC
- SMAC: Match specific source MAC address or Any
- Tag Type: Indicates tag type. Possible values are:
- Any: Match tagged and untagged frames
- Untagged: Match untagged frames
- Tagged: Match tagged frames
- C-Tagged: Match C-tagged frames
- S-Tagged: Match S-tagged frames
- VID: Indicates (VLAN ID), either a specific VID or range of VIDs. VID can be in the range of 1–4095 or Any.
- PCP: Priority Code Point. Valid values of PCP are specific (0, 1, 2, 3, 4, 5, 6, and 7) or range (0–1, 2–3, 4–5, 6–7, 0–3, and 4–7) or Any.
- DEI: Drop Eligible Indicator. Valid value of DEI is 0, 1 or Any.
- Frame Type: Indicates the type of frame. Possible values are:
- Any: Match any frame type
- Ethernet: Match EtherType frames
- LLC: Match (LLC) frames
- SNAP: Match (SNAP) frames
- IPv4: Match IPv4 frames
- IPv6: Match IPv6 frames
- Action: Indicates the classification action taken on ingress frame if the configured parameters are matched with the frame's content. The following are the possible actions:
- CoS: Classify Class of Service
- DPL: Classify Drop Precedence level
- DSCP: Classify DSCP value
- PCP: Classify PCP value
- DEI: Classify DEI value
- Policy: Classify ACL Policy number