4.4.2 CFM Domain Configuration
Configure CFM Domain parameters on the CFM Domain Configuration page, as shown in the following figure.

The CFM Domain Configuration page has the following parameters:
- Delete: Check to delete the entry. It is deleted during the next save.
- Domain: Name of Domain. Value is a single word which begins with an alphabetic letter A–Z or a–z with length 1–15.
- Format: Select the MD name format. To mimic Y.1731 MEG IDs, use type None.
- None
- String
- Name: The contents of this parameter
depend on the value of the format member. If format is None: Name is not used but is
set to all-zeros behind the scenes. This format is typically used by
Y.1731-kind-of-PDUs. If format is String: the name must contain a string from 1–43
characters long.
- None: Name is not used but is set to all-zeros behind the scenes. This format is typically used by Y.1731-kind-of-PDUs.
- String: the name must contain a string from 1–43 characters long.
- Level: MD/MEG level of this domain. Valid values are restricted to 0–7.
- TLV Option Select:
- Sender Id: Default Sender
ID TLV format to be used in CCMs generated by this domain (may be overridden
in service).
- None: Do not include Sender ID TLVs
- Chassis: Enable Sender ID TLV and send Chassis ID (MAC Address)
- Manage: Enable Sender ID TLV and send Management address (IPv4 Address)
- ChassisManage: Enable Sender ID TLV and send both Chassis ID (MAC Address) and Management Address (IPv4 Address)
- Defer: Let the global configuration decide if Sender ID TLVs are included (may be overridden in service)
- Port Status: Include or
exclude Port Status TLV in CCMs generated by this Domain or let higher level
determine (may be overridden in Service)
- Disable: Do not include Port Status TLVs
- Enable: Include Port Status TLVs
- Defer: Let the global configuration decide if Port Status TLVs are included (may be overridden in Service)
- Interface Status: Include
or exclude Interface Status TLV in CCMs generated by this Domain or let
higher level determine (may be overridden in Service)
- Disable: Do not include Interface Status TLVs
- Enable: Include Interface Status TLVs
- Defer: Let the global configuration decide if Interface Status TLVs are included (may be overridden in Service)
- Org. Specific: Exclude
Organization-Specific TLV in CCMs generated by this Domain or let higher
level determine (may be overridden in Service)
- Disable: Do not include Organization-Specific TLVs
- Defer: Let the global configuration decide if Organization-Specific TLVs are included (may be overridden in Service)
- Sender Id: Default Sender
ID TLV format to be used in CCMs generated by this domain (may be overridden
in service).