9.10.4 deprecated
The deprecated attribute causes the declaration to
which it is attached to be specially recognized by the compiler. When a
deprecated function or variable is used, the compiler will emit a
warning.
A deprecated definition is still defined and therefore
present in any object file. For example, compiling the following file:
int __attribute__((__deprecated__)) i;
int main() {
return i;
}
will produce the warning:
deprecated.c:4: warning: `i’ is deprecated (declared
at
deprecated.c:1)
i is still defined in the resulting object file in the
normal way.