6.5 Managing Path Sets
You can create and manage custom path sets for timing analysis and tracking purposes.
To manage path sets:
-
Right-click anywhere in the Domain Browser and choose Add
Set.
The Add Path Analysis Set dialog box appears.Tip: You can click the
icon in the SmartTime window bar to
display the Add Path Analysis Set dialog box.Figure 6-3. Add Path Analysis Set Dialog Box
- Enter a name for the path set.
- Select the source and sink pins. You can use the Using Filters to control the type of pins displayed.
-
Click OK.
The new path set appears below User Sets in the Domain Browser.
Figure 6-4. Updated Domain Browser with User Sets
-
To rename a path:
- Select the path set from User Sets in the Domain Browser.
- Right-click the set you want to rename, and then choose Rename Set from the right click menu.
- Edit the name directly in the Domain Browser.
-
To remove a path:
- Select the path set from User Sets in the Domain Browser.
- Right-click the set you want to delete, and then choose Delete Set from the right click menu.