4.1.2.4 Bluetooth®LE Transparent UART
This section helps users to create a peripheral device and send/receive characters between two connected Bluetooth LE devices over Microchip proprietary Transparent UART Profile. Peripheral device will be the PIC32WM-BW1 Curiosity board and central device can either be a Smart phone with Light Blue app or another PIC32WM-BW1 Curiosity board.
Users can choose to run the precompiled application example .hex file on
the PIC32WM-BW1 Curiosity board and experience the demo or go through
the steps involved in developing this application from scratch.
Hardware Requirement
| Tool | Qty |
|---|---|
| PIC32WM-BW1 Curiosity Board | 1 |
| Micro USB cable | 1 |
| USB Type-C™ Smart phone | 1 |
Software Requirement
- To install Tera Term tool, refer to the Tera Term web page listed in the Reference Documentation from Related Links.
Smart phone App
-
Light Blue iOS/Android app available in stores
Programming the Precompiled Hex File or Application Example
Programming the .hex File using MPLAB X IPE
- Import and program the precompiled
.hexfile is located in “<Harmony Content Path>\wireless_apps_pic32_bw1\apps\ble\peripheral\peripheral_trp_uart\hex” folder - For detailed steps, refer to
Programming a Device in MPLAB® IPE in Reference
Documentation from Related Links.Note: Ensure to choose the correct Device and Tool information.
Programming the Application using MPLAB X IDE
- Perform the following the steps mentioned in Running a Precompiled Example. For more information, refer to Running a Precompiled Application Example from Related Links.
- Open and program the application example
“
peripheral_trp_uart.X” located in “<Harmony Content Path>\wireless_apps_pic32_bw1\apps\ble\peripheral\peripheral_trp_uart\firmware” using MPLAB X IDE
Testing
- The application enables users to exchange data back and forth over UART between two BLE connected devices
- Program PIC32WM-BW1 Curiosity Board with
“
peripheral_trp_uart” application and open Tera Term configured at following settings through Terminal Settings:Terminal Settings- Baud Rate/Speed – 115200
- Parity – None
- Data Bits – 8
- Stop Bits – 1
- Flow Control – None
- Reset the board. Upon Reset, “BW1-Advertising” is displayed on the Tera Term.
- Launch the Light Blue mobile app and
search for the device name “pic32wm-bw1” and press Connect. When the connection is
established, the user will see “Connected” on Tera Term.
Figure 4-77. LightBlue® App - To send data from the PIC32WM-BW1 Curiosity Board (peripheral device) to the mobile app
(central device), select “
UUID: 49535343-1E4D-4BD9-BA61-23C647249616” then select Subscribe. - Change the data format to UTF-8 String in the Light Blue mobile app by clicking on Hex at the left top corner.
- Type characters on Tera Term emulator and the received data can be seen on the app under
Notified values. For example, in the above figure we see that when we send : “234” we see
that on the app.
Figure 4-78. Tera Term Logs - To send data to the PIC32WM-BW1 Curiosity Board (peripheral device) from the mobile app (central
device), select “
UUID: 49535343-8841-43F4-A8D4-ECBE34729BB3”. Change the data format to UTF-8 String as before.Note: When connecting through the LightBlue® app on Android, select the following properties: Write and Write Without Response. - Type a message like “Hi! Test” on the app and see it appearing on the Tera Term.
Figure 4-79. LightBlue® App - Users can use another PIC32WM-BW1 Curiosity Board configured as BLE Central Transparent UART instead of using a mobile app.
Project Graph
- Verify if the Project Graph window has all the expected configuration as illustrated in the following figure.
configUSE_TICKLESS_IDLE is
set to 0. The macro is available in FreeRTOSConfig.h
file.#define configUSE_TICKLESS_IDLE 0
Verifying Advertisement,Connection and Transparent UART Profile Configuration
-
Select BLE Stack component in project graph, to open component configuration and configure as illustrated in the following figure.
Figure 4-81. BLE Stack Configuration - Select Transparent Profile component in project graph, to open component configuration and configure as illustrated in the following figure.
Figure 4-82. Transparent Profile Configuration
Generating a Code
For more details on code generation, refer to MPLAB Code Configurator (MCC) Code Generation from Related Links.
Files and Routines Automatically Generated by the MCC
initialization.cThe BLE stack initialization routine executed during application initialization can be found in project files. This initialization routine is automatically generated by the MCC. This call initializes and configures the GAP, GATT, SMP, L2CAP and BLE middleware layers.
| Source Files | Usage |
|---|---|
app.c | Application State machine, includes calls for Initialization of all BLE stack (GAP,GATT, SMP, L2CAP) related component configurations |
app_ble\app_ble.c | Source Code for the BLE stack related component configurations,
code related to function calls from app.c |
app_ble\app_ble_handler.c | All GAP, GATT, SMP and L2CAP Event handlers |
app_ble\app_trsps_handler.c | All Transparent UART Server related Event handlers |
ble_trsps.c | All Transparent Server Functions for user application |
app.c is auto generated and has a state machine
based application code. Users can use this template to develop their own application.Header Files
ble_gap.h: Contains BLE GAP functions and is automatically included in theapp.cfile.ble_trsps.h: is associated with APIs and structures related to BLE Transparent Client functions for application user.
Function Calls
- MCC generates and adds the code to initialize the BLE Stack GAP, GATT, SMP and L2CAP in
APP_BleStackInit()function. APP_BleStackInit()is the API that will be called inside the Applications Initial State (APP_STATE_INIT) inapp.c.
User Application Development
- Include:
- Include the user action. For more information, refer to User Action from Related Links.
ble_trsps.hinapp.c, BLE Transparent UART Server related APIs.osal/osal_freertos_extend.hinapp_trsps_handler.c, OSAL related APIs are available here.definitions.hmust be included in all the files where UART will be used to print debug information.Note:definitions.his not specific to just UART but instead must be included in all the application source files where any peripheral functionality will be exercised.
-
Set Public Device Address in
app_ble.cinAPP_BleConfigBasic()BLE_GAP_Addr_T devAddr; devAddr.addrType = BLE_GAP_ADDR_TYPE_PUBLIC; devAddr.addr[5] = 0xC6; devAddr.addr[4] = 0xC5; devAddr.addr[3] = 0xC4; devAddr.addr[2] = 0xC3; devAddr.addr[1] = 0xC2; devAddr.addr[0] = 0xC1; // Configure device address BLE_GAP_SetDeviceAddr(&devAddr);
Figure 4-86. app_ble.c - Starting Advertisement in
app.c,APP_Tasks()caseAPP_STATE_INIT// Enable UART Read SERCOM0_USART_ReadNotificationEnable(true, true); // Set UART RX notification threshold to be 1 SERCOM0_USART_ReadThresholdSet(1); // Register the UART RX callback function SERCOM0_USART_ReadCallbackRegister(uart_cb, (uintptr_t)NULL); // Start Advertisement BLE_GAP_SetAdvEnable(0x01, 0x00); SERCOM0_USART_Write((uint8_t *)"BW1-Advertising\r\n",17);
Figure 4-87. app.c - Connected and Disconnected Events in
app_ble_handler.c- Connection handle associated with the peer peripheral device needs to be saved for data exchange after a BLE connection
-
p_event->eventField.evtConnect.connHandlehas this information#include "peripheral/sercom/usart/plib_sercom0_usart.h" extern uint16_t conn_hdl;
-
In
APP_BleGapEvtHandler(), caseBLE_GAP_EVT_CONNECTED:/* TODO: implement your application code.*/ SERCOM0_USART_Write((uint8_t *)"Connected\r\n",11); conn_hdl = p_event->eventField.evtConnect.connHandle;
-
In
APP_BleGapEvtHandler(), caseBLE_GAP_EVT_DISCONNECTED:/* TODO: implement your application code.*/ SERCOM0_USART_Write((uint8_t *)"Disconnected\r\n",14);
Figure 4-88. app_ble_handler.c - Transmit Data:
- Add
APP_MSG_UART_CBtoAPP_MsgId_Tenum inapp.hFigure 4-89. app.h BLE_TRSPS_SendData(conn_hdl , 1, &data);is the API to be used for sending data to the central device.- Example for transmitting over UART using the
BLE_TRSPS_SendData()API inapp.c#include "ble_trsps/ble_trsps.h" uint16_t conn_hdl;// connection handle info captured @BLE_GAP_EVT_CONNECTED event uint16_t ret; uint8_t uart_data; void uart_cb(SERCOM_USART_EVENT event, uintptr_t context) { APP_Msg_T appMsg; // If RX data from UART reached threshold (previously set to 1) if( event == SERCOM_USART_EVENT_READ_THRESHOLD_REACHED ) { // Read 1 byte data from UART SERCOM0_USART_Read(&uart_data, 1); appMsg.msgId = APP_MSG_UART_CB; OSAL_QUEUE_Send(&appData.appQueue, &appMsg, 0); } } void APP_UartCBHandler() { // Send the data from UART to connected device through Transparent service BLE_TRSPS_SendData(conn_hdl, 1, &uart_data); }
- In
APP_Tasks(), caseAPP_STATE_SERVICE_TASKS:else if(p_appMsg->msgId==APP_MSG_UART_CB) { // Pass BLE UART Data transmission target BLE UART Device handling APP_UartCBHandler(); }Figure 4-90. app.c
- Add
- Receive Data
BLE_TRSPS_EVT_RECEIVE_DATAis the event generated when data is sent from the central device- Use the
BLE_TRSPS_GetDataLength(p_event->eventField.onReceiveData.connHandle, &data_len);API to extract the length of the application data received BLE_TRSPS_GetData(p_event->eventField.onReceiveData.connHandle, data);API is used to retrieve the dataNote:BLE_TRSPS_Event_T p_eventstructure stores the information about BLE transparent UART callback functions.- Example for printing the received data from the central device over UART in
app_trsps_handler.c#include <string.h> #include "stdint.h" #include "ble_trsps/ble_trsps.h" #include "osal/osal_freertos_extend.h" #include "definitions.h"
- In
APP_TrspsEvtHandler(), caseBLE_TRSPS_EVT_RECEIVE_DATA:/* TODO: implement your application code.*/ uint16_t data_len; uint8_t *data; // Retrieve received data length BLE_TRSPS_GetDataLength(p_event->eventField.onReceiveData.connHandle, &data_len); // Allocate memory according to data length data = OSAL_Malloc(data_len); if(data == NULL) break; // Retrieve received data BLE_TRSPS_GetData(p_event->eventField.onReceiveData.connHandle, data); // Output received data to UART SERCOM0_USART_Write(data, data_len); // Free memory OSAL_Free(data);
Figure 4-91. app_trsps_handler.c