2.2 Project Resources
This window lists all the modules used in the project. To use a module, users need to select the module and click on the button (green cross) from the Device Resources list. By default, some of the modules are added in the Project Resources list, such as Device Family Pack (DFP), System. To remove a module from use or from the Project Resources list, select the module and then click on the button (red cross) appearing in the left top-side of the Project Resources window.
Note: The following MPLAB Harmony v3 modules
must be available in the Project Resources list:
- System
- DFP
- CMSIS (appears for Arm Cortex devices only)