37.8.1 Standby Sleep Mode
When the device enters the Standby Sleep mode, the system clock (SYS_CLK) is halted. If an ADC core selects SYS_CLK as its clock source or selects REFO3 as its clock source (REFO3 is generated from SYS-CLK) and the Standby Sleep mode occurs during a conversion, the conversion is aborted. The converter cannot resume a partially completed conversion on exiting from the Sleep mode. The ADC register contents are not affected by the device entering or leaving the Sleep mode. The ADC core can operate during the Sleep mode if the ADC clock source is derived from a source other than SYS_CLK that is active during the Sleep mode. The FRC clock source is a logical choice for operation during Sleep; however, the REFO3 clock source can also be used, provided it has an input clock that is operational during the Sleep mode.
ADC operation during the Sleep mode reduces the digital switching noise from the conversion. When the conversion is completed, the ARDYx status bit for that analog input is set and the result is loaded into the corresponding ADC Result register (ADCDATAx).
If any of the ADC interrupts are enabled, the device is woken up from the Sleep mode when the ADC interrupt occurs. The program execution resumes at the ADC ISR if the ADC interrupt is greater than the current CPU priority. Otherwise, execution continues from the instruction after the WFI instruction that placed the device in the Sleep mode.
To minimize the effects of digital noise on the ADC core operation, the user must select a conversion trigger source that ensures that the ADC take places in the Sleep mode. For example, the external interrupt pin (INT0) conversion trigger option (TRGSRC[4:0] = 00100) can be used for performing sampling and conversion while the device is in the Sleep mode.