1.4.2.8 mchp_correlate_q31()
void mchp_correlate_q31 (const q31_t * pSrcA, uint32_t srcALen, const q31_t * pSrcB, uint32_t srcBLen, q31_t * pDst)
Correlation of Q31 sequences.
| in | pSrcA |
points to the first input sequence. |
| in | srcALen |
length of the first input sequence. |
| in | pSrcB |
points to the second input sequence. |
| in | srcBLen |
length of the second input sequence. |
| out | pDst |
points to the block of output data Length 2 * max(srcALen, srcBLen) - 1. |
Note:
Implementation reverses pSrcB in-place before calling convolution. The const qualifier matches the ARM CMSIS-DSP API contract; callers should not rely on pSrcB being unmodified.