33.7.1 Data Bus Width
A data bus width of 8-bit or 16 bit can be selected for each chip select. This option is controlled by the DBW bit in the Mode register (SMC_MODE) for the corresponding chip select.
The following figure shows how to connect a 512-Kbyte × 8-bit memory on the NCS2.
The following figure shows how to connect a 512-Kbyte × 16-bit memory on NCS2.