33.7.3 NAND Flash Support
The SMC integrates circuitry that interfaces to NAND Flash devices.
The NAND Flash logic is driven by the SMC. Configuration is done via the SMC_NFCSx field in the CCFG_SMCNFCS register in the Bus Matrix. For details on this register, refer to the section “Bus Matrix (MATRIX)” of this data sheet. The external NAND Flash device is accessed via the address space reserved for the chip select programmed.
The user can connect up to four NAND Flash devices with separate chip selects.
The NAND Flash logic drives the read and write command signals of the SMC on the NANDOE and NANDWE signals when the NCSx programmed is active. NANDOE and NANDWE are disabled as soon as the transfer address fails to lie in the NCSx programmed address space.
- NCSx is active when CCFG_SMCNFCS.SMC_NFCSx = 1.
- When the NAND Flash logic is
activated, (SMC_NFCSx = 1), the NWE pin can be used only in Peripheral mode (NWE
function). If the NWE function is not used for other external memories (SRAM,
LCD), it must be configured in any one of the following modes:
- PIO input with pull-up enabled (default state after reset)
- PIO output set at level 1
The address latch enable and command latch enable signals on the NAND Flash device are driven by address bits A22 and A21of the address bus. Any bit of the address bus can also be used for this purpose. The command, address or data words on the data bus of the NAND Flash device use their own addresses within the NCSx address space (configured in the register CCFG_SMCNFCS in the Bus Matrix). The chip enable (CE) signal of the device and the ready/busy (R/B) signals are connected to PIO lines. The CE signal then remains asserted even when NAND Flash chip select is not selected, preventing the device from returning to Standby mode. The NANDCS output signal should be used in accordance with the external NAND Flash device type.
Two types of CE behavior exist depending on the NAND Flash device:
- Standard NAND Flash devices require that the CE pin remains asserted low continuously during the read busy period to prevent the device from returning to Standby mode. Since the SMC asserts the NCSx signal high, it is necessary to connect the CE pin of the NAND Flash device to a GPIO line, in order to hold it low during the busy period preceding data read out.
- This restriction has been removed for “CE don’t care” NAND Flash devices. The NCSx signal can be directly connected to the CE pin of the NAND Flash device.
The following figure illustrates both topologies: Standard and “CE don’t care” NAND Flash.