23.19 Recommended Programming Sequence
Follow the steps below to program the PMC:
- If the Main crystal oscillator is not required, the PLL and divider can be directly configured (Step 6.) else this oscillator must be started (Step 2.).
- Enable the Main crystal oscillator by setting CKGR_MOR.MOSCXTEN. The user can define a startup time. This can be done by configuring the appropriate value in CKGR_MOR.MOSCXTST. Once this register has been correctly configured, the user must wait for PMC_SR.MOSCXTS to be set. This can be done either by polling PMC_SR.MOSCXTS, or by waiting for the interrupt line to be raised if the associated interrupt source (MOSCXTS) has been enabled in PMC_IER.
- Switch MAINCK to the Main crystal oscillator by setting CKGR_MOR.MOSCSEL.
- Wait for PMC_SR.MOSCSELS to be set to ensure the switch is complete.
- Check MAINCK frequency:
This frequency can be measured via CKGR_MCFR.
Read CKGR_MCFR until the MAINFRDY field is set, after which the user can read CKGR_MCFR.MAINF by performing an additional read. This provides the number of Main clock cycles that have been counted during a period of 16 SLOW_CLK cycles.
If MAINF = 0, switch MAINCK to the Main RC Oscillator by clearing CKGR_MOR.MOSCSEL. If MAINF ≠ 0, proceed to Step 6.
- Set PLLA and Divider (if not required, proceed to Step 7.):
All parameters needed to configure PLLA and the divider are located in CKGR_PLLAR.
CKGR_PLLAR.DIVA is used to control the divider. This parameter can be programmed between 0 and 127. Divider output is divider input divided by DIVA parameter. By default, DIVA field is cleared which means that the divider and PLLA are turned off.
CKGR_PLLAR.MULA is the PLLA multiplier factor. This parameter can be programmed between 0 and 62. If MULA is cleared, PLLA will be turned off, otherwise the PLLA output frequency is PLLA input frequency multiplied by (MULA + 1).
CKGR_PLLAR.PLLACOUNT specifies the number of SLOW_CLK cycles before PMC_SR.LOCKA is set after CKGR_PLLAR has been written.
Once CKGR_PLLAR has been written, the user must wait for PMC_SR.LOCKA to be set. This can be done either by polling PMC_SR.LOCKA or by waiting for the interrupt line to be raised if the associated interrupt source (LOCKA) has been enabled in PMC_IER. All fields in CKGR_PLLAR can be programmed in a single write operation. If MULA or DIVA is modified, the LOCKA bit goes low to indicate that PLLA is not yet ready. When PLLA is locked, LOCKA is set again. The user must wait for the LOCKA bit to be set before using the PLLA output clock.
- Select MAIN_CLK and HCLK:
MAIN_CLK and HCLK are configurable via PMC_MCKR.
CSS is used to select the clock source of MAIN_CLK and HCLK. By default, the selected clock source is MAINCK.
PRES is used to define the HCLK and MAIN_CLK prescaler.s The user can choose between different values (1, 2, 3, 4, 8, 16, 32, 64). Prescaler output is the selected clock source frequency divided by the PRES value.
MDIV is used to define the MAIN_CLK divider. It is possible to choose between different values (0, 1, 2, 3). MAIN_CLK output is the HCLK frequency divided by 1, 2, 3 or 4, depending on the value programmed in MDIV.
By default, MDIV is cleared, which indicates that the HCLK is equal to MAIN_CLK.
Once the PMC_MCKR has been written, the user must wait for PMC_SR.MCKRDY to be set. This can be done either by polling PMC_SR.MCKRDY or by waiting for the interrupt line to be raised if the associated interrupt source (MCKRDY) has been enabled in PMC_IER. PMC_MCKR must not be programmed in a single write operation. The programming sequence for PMC_MCKR is as follows:
If a new value for PMC_MCKR.CSS corresponds to any of the available PLL clocks:
- Program PMC_MCKR.PRES.
- Wait for PMC_SR.MCKRDY to be set.
- Program PMC_MCKR.MDIV.
- Wait for PMC_SR.MCKRDY to be set.
- Program PMC_MCKR.CSS.
- Wait for PMC_SR.MCKRDY to be set.
If a new value for PMC_MCKR.CSS corresponds to MAINCK or SLCK:
- Program PMC_MCKR.CSS.
- Wait for PMC_SR.MCKRDY to be set.
- Program PMC_MCKR.PRES.
- Wait for PMC_SR.MCKRDY to be set.
If CSS, MDIV or PRES are modified at any stage, the MCKRDY bit goes low to indicate that MAIN_CLK and HCLK are not yet ready. The user must wait for MCKRDY bit to be set again before using MAIN_CLK and HCLK.
Note: If PLLA clock was selected as MAIN_CLK and the user decides to modify it by writing a new value into CKGR_PLLAR, the MCKRDY flag will go low while PLLA is unlocked. Once PLLA is locked again, LOCKA goes high and MCKRDY is set. While PLLA is unlocked, MAIN_CLK selection is automatically changed to SLOW_CLK for PLLA. For further information, see "Clock Switching Waveforms".MCK is MAINCK divided by 2.
- Select the Programmable clocks (PCKx):
PCKx are controlled via registers PMC_SCER, PMC_SCDR and PMC_SCSR.
PCKx can be enabled and/or disabled via PMC_SCER and PMC_SCDR. Three PCKx can be used. PMC_SCSR indicates which PCKx is enabled. By default all PCKx are disabled.
PMC_PCKx registers are used to configure PCKx.
PMC_PCKx.CSS is used to select the PCKx divider source. Several clock options are available:
- MAINCK
- SLOW_CLK
- MAIN_CLK
- PLLA_CLK
- UPLL_CLK_DIV
SLOW_CLK is the default clock source.
PMC_PCKx.PRES is used to control the PCKx prescaler. It is possible to choose between different values (1 to 256). PCKx output is prescaler input divided by PRES. By default, the PRES value is cleared which means that PCKx is equal to Slow clock.
Once PMC_PCKx has been configured, the corresponding PCKx must be enabled and the user must wait for PMC_SR.PCKRDYx to be set. This can be done either by polling PMC_SR.PCKRDYx or by waiting for the interrupt line to be raised if the associated interrupt source (PCKRDYx) has been enabled in PMC_IER. All parameters in PMC_PCKx can be programmed in a single write operation.
If the PMC_PCKx.CSS and PMC_PCKx.PRES parameters are to be modified, the corresponding PCKx must be disabled first. The parameters can then be modified. Once this has been done, the user must re-enable PCKx and wait for the PCKRDYx bit to be set.
- Enable the peripheral clocks.
Once all of the previous steps have been completed, the peripheral clocks can be enabled and/or disabled via registers PMC_PCERx and PMC_PCDRx.