23.11.4 Low-Power Mode Summary Table
The modes detailed above are the main low-power modes. Each part can be set to on or off separately and wake up sources can be individually configured. The following table provides a summary of the configurations of the low-power modes.
| Mode | SUPC, 32 kHz Oscillator, RTC, RTT Backup SRAM (BRAM), Backup Registers (GPBR), POR (Backup Area) | Regulator | Core Memory Peripherals | Mode Entry Configuration | Potential Wakeup Sources | Core at Wakeup | PIO State while in Low-Power Mode | PIO State at Wakeup | Wakeup Time (see Note 2) |
|---|---|---|---|---|---|---|---|---|---|
| Backup Mode | ON | OFF | OFF (Not powered) | SUPC_CR.VROFF = 1 SLEEPDEEP = 1 (see Note 1) | WKUP0–13 pins Supply Monitor RTC alarm RTT alarm | Reset | Previous state maintained | PIOA, PIOB, PIOC, PIOD & PIOE inputs with pullups | < 2 ms |
| Wait Mode w/Flash in Deep Power-down Mode | ON | ON | Powered (Not clocked) | PMC_MCKR.MDIV = 0 , CKGR_MOR.WAITMODE = 1 , SLEEPDEEP = 0 , PMC_FSMR.LPM = 1 , PMC_FSMR.FLPM = 1 (see Note 1) | WKUP0–13 pins
RTC RTT USBHS Processor debug (see Note 6) GMAC Wake on LAN event Wakeup from CAN (see Note 7) | Clocked back (see Note 3) | Previous state maintained | Unchanged | < 10 μs |
| Wait Mode w/Flash in Standby Mode | ON | ON | Powered (Not clocked) | PMC_MCKR.MDIV = 0 , CKGR_MOR.WAITMODE = 1 , SLEEPDEEP = 0 , PMC_FSMR.LPM = 1 , PMC_FSMR.FLPM = 0 (see Note 1) | WKUP0–13 pins RTC RTT USBHS Processor debug (see Note 6) GMAC Wake on LAN Wakeup from CAN (see Note 7) | Clocked back (see Note 3) | Previous state maintained | Unchanged | < 10 μs |
| Sleep Mode | ON | ON | Powered (Not clocked) (see Note 4) | WFI SLEEPDEEP = 0 PMC_FSMR.LPM = 0 (see Note 1) | Any enabled Interrupt | Clocked back | Previous state maintained | Unchanged | (see Note 5) |
Note:
- The SLEEPDEEP bit is in the Cortex-M7 System Control Register.
- When considering wakeup time, the time required to start the PLL is not taken into account. Once started, the device works with the Main RC oscillator. The user has to add the PLL startup time if it is needed in the system. The wakeup time is defined as the time taken for wakeup until the first instruction is fetched.
- HCLK = MAIN_CLK. The user may need to revert back to the previous clock configuration.
- Depends on MAIN_CLK frequency.
- In this mode, the core is supplied and not clocked. Some peripherals can be clocked.
- Resume from Wait mode if a debug request occurs (CDBGPWRUPREQ is set in the processor).
- CAN wake-up requires the use of any WKUP0–13 pin.