3.6.2 Architectural Overview
The FPU relies on the dsPIC33A CPU for all instruction fetches, most decoding and for all operand movement to and from the system memory. The FPU contains no local memory other than its own register set. Being coupled to the CPU, data size nomenclature is common to both CPU and FPU wherein a word is 16 bits wide, a long word is 32 bits wide and a double word is 64 bits wide.
FPU instructions are part of the CPU instruction set architecture and are executed as part of the CPU code image. FPU instructions are, therefore, executed as a part of the normal execution flow. There are no restrictions with regards to when FPU instructions may appear within the instruction flow.
The CPU can issue, and the FPU can accept, no more than one instruction per clock cycle. However, once issued, the CPU and FPU use independent pipelines to execute the instruction. Consequently, there can be multiple instructions in the process of being executed in both pipelines at any one time. The FPU pipeline will stall the CPU when it is unable to accept any more instructions. The FPU pipeline is also sensitive to speculative instruction control from the CPU (i.e., such that not all issued FPU instructions will be committed). This allows FPU instructions to be located within speculative execution slots that follow conditional branches.
After a successful issue of an FPU instruction, the CPU continues as if executing a single cycle FNOP instruction, and the FPU instruction execution continues within the FPU. Therefore, as some FPU instructions require several cycles to complete, subsequent CPU (and/or FPU) instructions can be fetched, issued and executed (dependencies aside) while the FPU operation progresses. Only when the CPU encounters a hazard with the FPU will it be stalled until the hazard is resolved.
Data and structural hazards are detected and mitigated in both the CPU and FPU and can result in operational stalls which will extend the execution time and increase the effective cycles per instruction of both CPU and FPU instructions.