2.3.3.4 Customizing the I/O
(Ask a Question)A five-bit programmable input delay element is associated with each I/O. The value of this delay is set on a bank-wide basis (see the following table). It is optional for each input buffer within the bank (that is, the user can enable or disable the delay element for the I/O). When the input buffer drives a register within the I/O, the delay element is activated by default to ensure a zero hold-time. The default setting for this property can be set in Designer. When the input buffer does not drive a register, the delay element is deactivated to provide higher performance. Again, this can be overridden by changing the default setting for this property in Designer.
The slew-rate value for the LVTTL output buffer can be programmed and can be set to either slow or fast.
The following table lists the values of bank-wide delay.
| Bits Setting | Delay (ns) |
|---|---|
| 0 | 0.54 |
| 1 | 0.65 |
| 2 | 0.71 |
| 3 | 0.83 |
| 4 | 0.9 |
| 5 | 1.01 |
| 6 | 1.08 |
| 7 | 1.19 |
| 8 | 1.27 |
| 9 | 1.39 |
| 10 | 1.45 |
| 11 | 1.56 |
| 12 | 1.64 |
| 13 | 1.75 |
| 14 | 1.81 |
| 15 | 1.93 |
| 16 | 2.01 |
| 17 | 2.13 |
| 18 | 2.19 |
| 19 | 2.3 |
| 20 | 2.38 |
| 21 | 2.49 |
| 22 | 2.55 |
| 23 | 2.67 |
| 24 | 2.75 |
| 25 | 2.87 |
| 26 | 2.93 |
| 27 | 3.04 |
| 28 | 3.12 |
| 29 | 3.23 |
| 30 | 3.29 |
| 31 | 3.41 |
These values are minimum drive strengths.