4 Revision History

The revision history describes the changes that were implemented in the document. The changes are listed by revision, starting with the most current publication.
Table 4-1. Revision History
RevisionDateDescription
B06/2025The following is the list of changes in revision B of the document:
A10/2024The following is the list of changes in revision A of the document:
1803/2012The following is the list of changes in revision 18 of the document:
  • Updated Table 2-1 to correct the maximum DC core supply voltage (VCCA) from 1.6 V to 1.7 V (SAR 36786). The maximum input voltage (VI) was corrected from 3.75 V to 4.1 V (SAR 35419).
  • Added values for tristate leakage current IOZ, and IIH and IIL in table Table 2-3 (SARs 35774, 32021).
  • Figure 2-2 was updated to correct the units for the resistance from "W" to Ω (SAR 36415).
  • In User I/Os2 section, the following sentence was added to clarify the slew rate setting (SAR 34943): The slew rate setting is effective for both rising and falling edges.
  • Figure 2-3 was revised to show the VCCI and GND clamp diodes. The explanatory text above the figure was revised as well (SAR 34942).
  • Equation for 5 V tolerance was corrected to change Vdiode from 0.6 V to 0.7 V (SAR 36786).
  • Additional information was added to the Using the Weak Pull-Up and Pull-Down Circuits section to clarify how the weak pull-up and pull-down resistors are physically implemented (SAR 34945).
  • The description for the CINCLK parameter in Table 2-23 was changed from "Input capacitance on clock pin" to "Input capacitance on HCLK and RCLK pin" (SAR 34944).
  • Table 2-24 is new (SAR 34942).
  • The minimum VIL for 1.5 V LVCMOS and PCI was corrected from –0.5 to –0.3 in Table 2-34 and Table 2-37 (SAR 34358).
  • Support for simulating the GCLR/ GPSET feature in the Axcelerator Family was added in Libero software v9.0 SPI1. Reference to the section explaining this in the Antifuse Macro Library Guide was added to the R-Cell (SAR 26413).
  • The enable signal in Figure 2-33 was corrected to show it is active low rather than active high (SAR 34946).
1709/2011The following is the list of changes in revision 17 of the document:
  • The versioning system for datasheets has been changed. Datasheets are assigned a revision number that increments each time the datasheet is revised.

    The Axcelerator Family Device Status table indicates the status for each device in the device family.

  • The Features section, Programmable Interconnect Element section, and Security section were revised to clarify that although no existing security measures can give an absolute guarantee, Microsemi FPGAs implement the best security available in the industry (SAR 32865).
  • The C180 package was removed from product tables and the Package Pin Assignments section (PDN 0909).
  • Package names used in the Table 3-1 and Package Pin Assignments section were revised to match standards given in Package Mechanical Drawings (SAR 27395).
  • The section User I/Os2 was updated as follows: "The user does not need to assign VREF pins for OUTBUF and TRIBUF. VREF pins are needed only for input and bidirectional I/Os" (SARs 24181, 24309).
  • Power values in Table 2-4 were updated to reflect those of SmartPower (SAR 33945).
  • Two parameter names were corrected in Figure 2-10.

    One occurrence of tENLZ was changed to tENZL and one occurrence of tENHZ was changed to tENZH (SAR 33890).

  • The Timing Model section was updated with new timing values. Timing tables in the I/O Specifications section were updated to include enable paths. Values in the timing tables in the Voltage-Referenced I/O Standards section and Differential Standards section were updated.
  • Table 2-67 was updated (SAR 33945).
  • Figure 2-11 was replaced (SAR 33043).
  • The timing tables for RAM and FIFO were updated (SAR 33945).
  • "Data Registers (DRs)" values were modified for IDCODE and USERCODE (Data Registers (DRs) SARs 18257, 26406).
  • The package diagram for the CQ208 package was incorrect and has been replaced with the correct diagram (SARs 23865, 26345).
1610/2010The following is the list of changes in revision 16 of the document:
  • The datasheet was updated to include AX2000-CQ2526 information.
  • MIL-STD-883 Class B is no longer supported by Axcelerator FPGAs and as a result was removed.
  • A footnote was added to the Axcelerator Clock Management System section.
1511/2008The following is the list of changes in revision 15 of the document:
  • RoHS-compliant information was added to the Ordering Information.
  • ACTgen was changed to SmartGen because ACTgen is obsolete.
14—The following is the list of changes in revision 14 of the document:
13—The following is the list of changes in revision 13 of the document:
12—The following is the list of changes in revision 12 of the document:
11—The following is the list of changes in revision 11 of the document:
10—The following is the list of changes in revision 10 of the document:
9.0—The following is the list of changes in revision 9.0 of the document:
8.0—The following is the list of changes in revision 8.0 of the document:
7.0—The following is the list of changes in revision 7.0 of the document:
6.0—The following is the list of changes in revision 6.0 of the document:
5.0—The following is the list of changes in revision 5.0 of the document:
  • In the PQ208 table, pin 196 was missing, but it has been added in this version with a function of GND.
  • The following pins in the FG484 table for AX500 were changed:

    Pin G7 is GND/LP Pins AB8, C10, C11, C14, AB16 are NC.

  • The FG676 table was updated.
4.0—The following is the list of changes in revision 4.0 of the document:
3.0—The following is the list of changes in revision 3.0 of the document: