9.6 Run Program Action
(Ask a Question)To program the PolarFire device, perform the following steps:
- Ensure that the jumper settings on the board are as listed in the following table.
Table 9-3. PolarFire® Evaluation Board Jumper Settings Jumper Description J18, J19, J20, J21, and J22 Short pin 2 and 3 for programming the PolarFire® FPGA through FTDI J28 Short the pin 2 and 3 for programming through the on-board FlashPro5 J4 Short pin 1 and 2 for manual power switching using SW3 J12 Short pin 3 and 4 for 2.5V J46 Short pin 1 and 2 for routing 125 MHz differential clock oscillator output to the side. Open pin 1 and 2 for routing 122.88 MHz differential clock oscillator to the line side. - Connect the power supply cable to the J9 connector.
- Connect the USB cable from the host PC to the J5 (FTDI port).
- Power ON the board using the SW3 slide switch.
The following figure shows the board setup.
Figure 9-9. PolarFire® Evaluation Board Setup - On the Design Flow window, double-click Run PROGRAM Action.
The device is successfully programmed and a green tick mark appears next to Run PROGRAM Action, see Figure 9-1. LED 4 is asserted once the device is programmed.