30.4.4 Step Queue Pointer
The PTG Step Queue Pointer register (PTGQPTR) addresses the currently active step command
in the step queue. While the PTG is not executing step commands (PTGSTRT =
0), any value can be written to PTGQPTR regardless of the state of
the ON bit. Once the PTGSTRT bit is set, the PTG begins executing step commands at the
queue location indicated by PTGQPTR, and the register becomes read-only. When the PTG is
disabled, the PTGQPTR register is cleared once on transition of the ON bit from
‘1’ to ‘0’, after which PTGQPTR becomes writable
again.
0) and Idle state (ON = 1 and PTGSTRT =
0), a read returns the index of the first step command to execute.
In the Active state (ON = 1 and PTGSTRT = 1), a read
returns the index of the currently executing step command. The PTGQPTR register is
typically incremented during the first cycle of each command. The exceptions to this
rule are:- If the
PTGJMPcommand is executed: The Step Queue Pointer is loaded with the target queue address. - If the
PTGJMPCxcommand is executed and PTGCx is less than PTGCxLIM: The Step Queue Pointer is loaded with the target queue address. - If PTGQPTR points to the last
step command in PTGQUEn: The Step Queue Pointer will roll over to
‘
0’.