23.5.1 Interrupt Configuration
Each SPI module has three dedicated interrupt flag bits: SPIxIF, SPIxRXIF and SPIxTXIF, and corresponding interrupt enable bits, SPIxIE, SPIxRXIE and SPIxTXIE. These bits are used to determine the source of an interrupt and to enable or disable an individual interrupt source. Note that all the interrupt sources for a specific SPI module share one interrupt vector. Each SPI module can have its own priority level independent of other SPI modules.
The SPIxIE, SPIxTXIE and SPIxRXIE bits are used to define the behavior of the interrupt controller when a corresponding SPIxIF, SPIxTXIF or SPIxRXIF bit is set. When the corresponding interrupt enable bit is clear, the interrupt controller does not generate a CPU interrupt for the event. If the interrupt enable bit is set, the interrupt controller will generate an interrupt to the CPU when the corresponding interrupt flag bit is set (subject to the priority).
It is the responsibility of the user’s software routine that services a particular interrupt to clear the appropriate interrupt flag bit before the service routine is complete.
The priority of each SPI module can be set independently with the SPIxIP[2:0] bits. This priority defines the priority group to which the interrupt source will be assigned. The priority groups range from a value of seven (the highest priority), to a value of zero (which does not generate an interrupt). An interrupt being serviced will be preempted by an interrupt in a higher priority group.
The priority group bits allow more than one interrupt source to share the same priority. If simultaneous interrupts occur in this configuration, the natural order of the interrupt sources within a priority group pair determines the interrupt generated. The natural priority is based on the vector numbers of the interrupt sources. The lower the vector number, the higher the natural priority of the interrupt. Any interrupts that were overridden by natural order will then generate their respective interrupts based on priority and natural order, after the interrupt flag for the current interrupt is cleared.
After an enabled interrupt is generated, the CPU will jump to the vector assigned to that interrupt. The vector number for the interrupt is the same as the natural order number. The CPU will then begin executing code at the vector address. The user’s code at this vector address should perform any application-specific operations required and clear interrupt flags, SPIxIF, SPIxTXIF or SPIxRXIF, and then exit.
With Enhanced Buffering mode, the user application should clear the interrupt request flag after servicing the interrupt condition.
If an SPIx interrupt has occurred, the ISR should read the SPIx Data Buffer (SPIxBUF) register and then clear the SPIx interrupt flag.