14.6 Interrupts
Each DMA channel has its own set of four interrupt flags, used to indicate a range of conditions during and following data transfers. Setting any of these flags with an interrupt event causes the device-level DMA Channel x Interrupt Flag (DMAxIF) to be set. With one exception, these flags are always enabled and not configurable. The DMAxIE bits, located in the IECx interrupt registers, will determine if a device-level interrupt is actually generated.
Since any of the DMA channel’s individual event flags can trigger a device-level interrupt for the channel, the user must include a method within the ISR to determine which flag triggered the interrupt.
- DMA completion interrupt
- DMA halfway point interrupt
- Overrun interrupt
- Pattern match interrupt
- Address Fault
- Bus write error
- Bus read error
In all of these conditions, the DMA will suspend its operation and the CHEN bit will be cleared.