26.4.4.2 Addressed Communication

The Addressed Command mode is the same as the Broadcast mode, except instead of ‘0’ in IDSx, an actual address is used. This will send a command to the specific client addressed. For an example, see Addressed Command Code Example.