32.4.3 Operating Range
The maximum voltage that can be developed across a resistor driven by a current source depends on AVDD and the other voltage sources in the circuit.
When the resistor is connected to AVSS, such as seen in Figure 32-2, the maximum voltage that can be developed is approximately AVDD. However, when the developed voltage is greater than the current source’s internal threshold, the output current is reduced. To prevent this, the maximum developed voltage across RESD + REXT should be limited to AVDD – 0.5V (typical) with respect to the output current value.