23.2.2 Message Protocol
A typical I2C message is illustrated in Figure 23-3. In this example, the message will read a specified byte from a 24LC256 I2C serial EEPROM. The I2C device will act as the host, and the 24LC256 device will act as the client.
Figure 23-3 illustrates the data as driven by the host device and the client device, taking into account that the combined SDAx line is a wired-AND of the host and client data. The host device controls and sequences the protocol. The client device will only drive the bus at specifically determined times.