16.5.9.3.2 Frequency Scaling
Frequency scaling provides the ability to drop clocks to effectively stretch the period or duty cycle and is useful for resonant power control applications that require a variable frequency control input. The clock input for the frequency scaling circuit is chosen using the MCLKSEL bits (PCLKCON[1:0]). The frequency scaling clock output is available to each PWM Generator and can be selected using the CLKSEL[1:0] control bits (PGxCON[4:3]).
The FSCL (Frequency Scale) and FSMINPER (Frequency Scaling Minimum Period) registers specify the amount of frequency scaling and are readable/writable at all times. The frequency scaling circuit performs modulo arithmetic where the FSCL value is constantly accumulated until the sum is larger than the FSMINPER register value. When the sum becomes larger than the FSMINPER register value, a clock pulse is produced and the accumulated value is reduced by the value in the FSMINPER register, as shown in Figure 16-36.
Note that the frequency scaling signal is applied only to the PWM time base counter and does not affect the operation of the dead time or the LEB counters. The frequency scaling circuit remains in a Low-Power state if not selected by any of the PWM Generators.
Example: Frequency Scaling Calculation
Where:
FSCL ≤ FSMINPER