25.2.4.8 Time-out
Once all data have been sent in addition to the optional bits, there should be a time-out
on the SLO line while the host transmits the CDM bit. In the BiSS time-out, no further
clock pulses are sent to the MA by the host. The Inverse state of the MA line during the
BiSS time-out is the state of the CDM bit. At the end of the data transmission, the host
sets its output MO to the Idle state ‘1’. The clients then pass on this
‘1’ received at SLI to their output SLO as soon as they have
detected the expiration of the time-out. This ensures the BiSS time-out on the line SL
is only signaled to the host when all connected clients have detected the time-out. When
the BiSS time-out expires, all clients return to the Idle state; all lines are set to
the high signal level (‘1’) in the process.