25.4.2.4 Transmitting Sensor Data

To summarize the following sections, use the following steps and the Sensor Communication Code Example.

  1. Configure BiSS PPS.
  2. Configure the SCD frequency and getsense frequency.
  3. Select the client location, the protocol used on the channel and determine if the client device is a sensor or an actuator.
  4. Configure the SCD length.
  5. Configure the CRC used and the CRC length.
  6. Turn the module on.
  7. Initialize the BiSS module and poll INSTRWA (can read B1SCDATAxX now if line delay calculations are desired later).
  8. Turn AGS on.
  9. Poll end of transmission, EOT, Status bit and/or CRC Valid bit to confirm a successful transmission.
  10. Read the value from B1SCDATAxX.