29.4.10.3 PTG Step Interrupt
After each step command is executed in Single-Step mode, the PTG step interrupt will occur, if enabled. This notifies the application of the completion of the command.
Single-Step Demonstration Program
//This code shows a basic example of using PTG Single-Step Mode.
//Program must be run in Debug Mode.
//Once the PTGSSEN bit is set, press the push button (RF1) to set PTGSTRT to execute a single command.
//An LED (RC8) will toggle on the completion of each command.
#include <xc.h>
void PTG_populate_queue() {
//Set up commands in the PTG Step Queue
PTGQUE0bits.STEP0 = 0; //NOP
PTGQUE0bits.STEP1 = 0b10100000; //PTGJMP(0)
}
int main (void) {
_ANSELC1 = 0;
_TRISC1 = 1; //RC1 input connected to push button switch
_Bool sw_latch = 0; //Latch button input so one press makes one step
_TRISC8 = 0; //RC8 output connected to external indicator
_LATC8 = 0; //RC8 output low initially
PTG_populate_queue(); //Set up step commands in PTG queue
PTGCONbits.ON = 1; //Place breakpoint on this line. When execution halts,
//set PTGSSEN = 1 using the debugger, then continue.
_PTGSTEPIE = 1; //Enable PTG Step Interrupt
while(1) {
if (!_RC1) { //Check if button is pressed (active low)
if (!sw_latch) {
_PTGSTRT = 1; //Execute a single Step command
sw_latch = 1;
}
}
else {
sw_latch = 0; //Reset latch for next button press
}
}
return 0;
}
void __attribute__ ((__interrupt__)) _PTGSTEPInterrupt(void) {
_LATC8 = !_LATC8; //Toggle RC8 to show step has taken place
_PTGSTEPIF = 0;
}