15.5.2.6.5 PCI Acceptance Logic
PCI acceptance logic is the selectable logic function that is applied to the PCI inputs. The six types of available logic functions shown in Figure 15-21 are:
- PCI Level mode: The PCI signal is passed directly through for use by the PWM Generator. The PCI signal may be optionally qualified (ANDed) with an acceptance qualifier signal.
- PCI Rising Edge mode: The PCI signal is passed through a rising edge detection circuit that generates a pulse event. The PCI signal may be optionally qualified (ANDed) with an acceptance qualifier signal.
- PCI Any Edge mode: The PCI signal is passed through both rising and falling edge detection circuits that generate a pulse event on either edge transition. The PCI signal may be optionally qualified (ANDed) with an acceptance qualifier signal.
- PCI Latched mode: The PCI signal is used to set an SR latch. In this mode, a terminator signal and optional terminator qualifier are used to reset the latch. The entry into the PCI Active state is asynchronously latched and possibly gated by a qualifier signal. The exit from the PCI Active state is determined by a terminator signal and possibly a terminator qualifier signal. The exit from the PCI Active state can also be qualified by the absence of the PCI signal itself. (This is particularly important when the Latched mode is used for Fault control applications.)
- PCI Latched Rising Edge mode: The PCI signal is passed through a rising edge detect circuit and optionally qualified to create a pulse event. This pulse event is used to set an SR latch. The SR latch can be reset in a similar fashion to the Latched mode. The Latched Edge Detect mode allows the PCI to become active on a PCI edge event after a qualifier signal is present.
- PCI Latched Any Edge mode: This mode is similar to Latched Rising Edge mode except that either a rising or falling edge is used to create the pulse event to set the latch.
- Qualifier Latched Rising Edge mode: Similar to PCI Latched Rising Edge mode except that the PCI and qualifier signals are interchanged.
- Qualifier Latched Any Edge mode: Similar to PCI Latched Any Edge mode except that PCI and qualifier signals are interchanged.
Each mode of the PCI logic is intended to target a particular kind of power control function, although the functions can be applied to a wide variety of applications. The Level mode is useful when the PCI signals are used to affect the state of the PWM outputs asynchronously. For example, the Level mode could be used to allow an external blanking signal to force the PWM output pins to a specific state for a period of time.
The Edge Event mode is useful when a PCI signal is used to synchronize a PWM Generator time base to an external source. When the PCI logic is used as a synchronization function, the rising edge event of the PCI signal is of primary interest. The edge event causes the PCI logic to generate an internal pulse which triggers a PWM Generator.
The Latched mode is useful for Fault and current-limiting applications. In these applications, it is important for the PCI logic to enter the Active state asynchronously when qualified. The PCI logic will remain active until a selected terminating event occurs. Usually, the terminating event is a software action (manual) or the end of a PWM cycle (automatic). The Latched Edge Detect mode is useful for some types of current control applications. The PCI output cannot become active until a transition of the PCI input occurs after a qualifying condition.
Latching Mode Control
By default, the SR latch used in Latched Acceptance modes is set-dominant. This prevents a reset of the SR latch if the PCI signal is active when the termination event signal is asserted. The LATMOD control bit (PGxyPCI1[20]) can be used to create a Reset-dominant SR latch for certain PWM control functions. It is not recommended to use a Reset-dominant SR latch when the PCI logic is used to handle Fault conditions as this could allow the Active state of the PCI logic to be reset while the PCI input signal is still active. Examples of Latched modes are shown in Figure 15-23.