4.9.5 Expression Formatting
The Microchip Studio debugger includes expression evaluators that work when entering an expression in the QuickWatch and Watches, Memory View, Watch Window or Immediate window. The expression evaluators are also at work in the Breakpoints window and many other places in the debugger.
General Syntax:
Val, formatString
Format Specifier for Values
The following tables show the format specifiers recognized by the debugger.
Specifier | Format | Expression | Value Displayed |
|---|---|---|---|
d,i | Signed decimal integer | 0xF000F065, d | -268373915 |
u | Unsigned decimal integer | 0x0065, u | 101 |
b | Unsigned binary number | 0xaa,b2 | 0b10101010 |
o | Unsigned octal integer | 0xF065, o | 0170145 |
x,X | Hexadecimal integer | 61541, x | 0x0000F065 |
1,2,4,8 | As a suffix specifying number of bytes for: d, i, u, o, x, X. | 00406042,x2 | 0x0c22 |
s | String | 0x2000, s | 'Hello World' |
f | Signed floating point | (3./2.), f | 1.500000 |
e | Signed scientific notation | (3./2.), e | 1.500000e+000 |
g | Signed floating point or signed scientific notation, whichever is shorter | (3./2.), g | 1.5 |
c | Single character | 0x0065, c | 101 'e' |
Size Specifier for Pointers as Arrays
If you have a pointer to an object you want to view as an array, you can use an integer to specify the number of array elements:
ptr,10 or array,20
Memory Type Specifier
The following memory type specifiers will force the memory reference to a specific memory type. To be used in the memory window in the address field, you should have a pointer to an object you want to view as an array. You can use an integer to specify the number of the array elements:
Specifier | Expression | Value Displayed |
|---|---|---|
Flash or program | Program memory | 0,Flash |
data | Data memory | 0x2000,data |
sram | SRAM | 0x100,sram |
reg or registers | Registers | 1,reg |
io, eeprom, fusebytes, lockbytes, signature, usersign, prodsign | Memory types with same names |