DRV_W25_Initialize Function
C
SYS_MODULE_OBJ DRV_W25_Initialize
(
const SYS_MODULE_INDEX drvIndex,
const SYS_MODULE_INIT *const init
);Summary
Initializes the W25 Driver
Description
This routine initializes the W25 driver making it ready for client to use.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| drvIndex | Identifier for the instance to be initialized |
| init | Pointer to a data structure containing any data necessary to initialize the driver. |
Returns
If successful, returns a valid handle to a driver instance object. Otherwise it returns SYS_MODULE_OBJ_INVALID.
Example
// This code snippet shows an example of initializing the W25 Driver
// with W25256JV flash device attached.
SYS_MODULE_OBJ objectHandle;
const DRV_W25_PLIB_INTERFACE drvW25PlibAPI =
{
.Write = QMSPI0_Write,
.Read = QMSPI0_Read,
.DMATransferRead = QMSPI0_DMATransferRead,
.DMATransferWrite = QMSPI0_DMATransferWrite
};
const DRV_W25_INIT drvW25InitData =
{
.w25Plib = &drvW25PlibAPI,
};
objectHandle = DRV_W25_Initialize((SYS_MODULE_INDEX)DRV_W25_INDEX, (SYS_MODULE_INIT *)&drvW25InitData);
if (SYS_MODULE_OBJ_INVALID == objectHandle)
{
// Handle error
}Remarks
This routine must be called before any other W25 driver routine is called.
This routine should only be called once during system initialization. This routine will block for hardware access.