DRV_W25_SectorErase Function
C
bool DRV_W25_SectorErase( const DRV_HANDLE handle, uint32_t address );Summary
Erase the sector from the specified block start address.
Description
This function schedules a non-blocking sector erase operation of flash memory. Each Sector is of 4 KByte.
The requesting client should call DRV_W25_TransferStatusGet() API to know the current status of the request.
Preconditions
The DRV_W25_Open() routine must have been called for the specified W25 driver instance.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| address | block start address from where a sector needs to be erased. |
Returns
true
- if the erase request is successfully sent to the flash
false
- if Write enable fails before sending sector erase command to flash
- if sector erase command itself fails
Example
DRV_HANDLE handle; // Returned from DRV_W25_Open
uint32_t sectorStart = 0;
if(DRV_W25_SectorErase(handle, sectorStart) == false)
{
// Error handling here
}
// Wait for erase to be completed
while(DRV_W25_TRANSFER_BUSY == DRV_W25_TransferStatusGet(handle));
Remarks
This routine will block wait until erase request is submitted successfully.
Client should wait until erase is complete to send next transfer request.