1.1.13.3.4 Library Interface
W25 driver library provides the following interfaces:
Functions
| Name | Description |
|---|---|
| DRV_W25_Initialize | Initializes the W25 Driver |
| DRV_W25_Open | Opens the specified W25 driver instance and returns a handle to it |
| DRV_W25_Close | Closes an opened-instance of the W25 driver |
| DRV_W25_Status | Gets the current status of the W25 driver module |
| DRV_W25_UnlockFlash | Unlocks the flash device for Erase and Program operations |
| DRV_W25_ReadJedecId | Reads JEDEC-ID of the flash device |
| DRV_W25_SectorErase | Erase the sector from the specified block start address |
| DRV_W25_BlockErase | Erase a block from the specified block start address |
| DRV_W25_ChipErase | Erase entire flash memory |
| DRV_W25_Read | Reads n bytes of data from the specified start address of flash memory |
| DRV_W25_PageWrite | Writes one page of data starting at the specified address |
| DRV_W25_TransferStatusGet | Gets the current status of the transfer request |
| DRV_W25_GeometryGet | Returns the geometry of the device |
Data types and constants
| Name | Type | Description |
|---|---|---|
| DRV_W25_TRANSFER_STATUS | Enum | W25 Driver Transfer Status |
| DRV_W25_GEOMETRY | Struct | W25 Device Geometry data |