DRV_W25_Status Function
C
SYS_STATUS DRV_W25_Status( const SYS_MODULE_INDEX drvIndex );Summary
Gets the current status of the W25 driver module.
Description
This routine provides the current status of the W25 driver module.
Preconditions
Function DRV_W25_Initialize should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| drvIndex | Identifier for the instance used to initialize driver |
Returns
SYS_STATUS_READY - Indicates that the driver is ready and accept requests for new operations.
SYS_STATUS_UNINITIALIZED - Indicates the driver is not initialized.
SYS_STATUS_BUSY - Indicates the driver is in busy state.
Example
SYS_STATUS Status;
Status = DRV_W25_Status(DRV_W25_INDEX);
if (status == SYS_STATUS_READY)
{
// W25 driver is initialized and ready to accept requests.
}Remarks
This routine will NEVER block wait for hardware.