DRV_MX25L_ChipErase Function
C
bool DRV_MX25L_ChipErase( const DRV_HANDLE handle );Summary
Erase entire flash memory.
Description
This function schedules a non-blocking chip erase operation of flash memory.
The requesting client should call DRV_MX25L_TransferStatusGet() API to know the current status of the request.
The request is sent in QUAD_MODE to flash device.
Preconditions
The DRV_MX25L_Open() routine must have been called for the specified MX25L driver instance.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
Returns
true
- if the erase request is successfully sent to the flash
false
- if Write enable fails before sending sector erase command to flash
- if chip erase command itself fails
Example
DRV_HANDLE handle; // Returned from DRV_MX25L_Open
if(DRV_MX25L_ChipErase(handle) == false)
{
// Error handling here
}
// Wait for erase to be completed
while(DRV_MX25L_TransferStatusGet(handle) == DRV_MX25L_TRANSFER_BUSY);
Remarks
This routine will block wait until erase request is submitted successfully.
Client should wait until erase is complete to send next transfer request.