DRV_MX25L_GeometryGet Function
C
bool DRV_MX25L_GeometryGet( const DRV_HANDLE handle, MX25L_GEOMETRY *geometry );Summary
Returns the geometry of the device.
Description
This API gives the following geometrical details of the MX25L Flash:
- Number of Read/Write/Erase Blocks and their size in each region of the device
- Flash block start address.
Precondition
The DRV_MX25L_Open() routine must have been called for the specified MX25L driver instance.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| *geometry_table | pointer to flash device geometry table instance |
Returns
true - if able to get the geometry details of the flash
false - if read device id fails
Example
DRV_HANDLE handle; // Returned from DRV_MX25L_Open DRV_MX25L_GEOMETRY mx25lFlashGeometry; uint32_t readBlockSize, writeBlockSize, eraseBlockSize; uint32_t nReadBlocks, nReadRegions, totalFlashSize; DRV_MX25L_GeometryGet(handle, &mx25lFlashGeometry); readBlockSize = mx25lFlashGeometry.read_blockSize; nReadBlocks = mx25lFlashGeometry.read_numBlocks; nReadRegions = mx25lFlashGeometry.numReadRegions; writeBlockSize = mx25lFlashGeometry.write_blockSize; eraseBlockSize = mx25lFlashGeometry.erase_blockSize; totalFlashSize = readBlockSize * nReadBlocks * nReadRegions;
Remarks
This API is more useful when used to interface with block driver like memory driver.