DRV_MX25L_TransferStatusGet Function
C
DRV_MX25L_TRANSFER_STATUS DRV_MX25L_TransferStatusGet( const DRV_HANDLE handle );Summary
Gets the current status of the transfer request.
Description
This routine gets the current status of the transfer request. The application must use this routine where the status of a scheduled request needs to be polled on.
Preconditions
The DRV_MX25L_Open() routine must have been called for the specified MX25L driver instance.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
Returns
DRV_MX25L_TRANSFER_ERROR_UNKNOWN - If the flash status register read request fails
DRV_MX25L_TRANSFER_BUSY - If the current transfer request is still being processed
DRV_MX25L_TRANSFER_COMPLETED - If the transfer request is completed
Example
DRV_HANDLE handle; // Returned from DRV_MX25L_Open
if (DRV_MX25L_TransferStatusGet(handle) == DRV_MX25L_TRANSFER_COMPLETED)
{
// Operation Done
}Remarks
This routine will block for hardware access.