1.2.4.4.8 SYS_CONSOLE_Flush Function
1.2.4.4.8 C
bool SYS_CONSOLE_Flush(const SYS_CONSOLE_HANDLE handle)
1.2.4.4.8 Summary
Flushes the read and write queues for the given console instance.
1.2.4.4.8 Description
This function flushes the read and write buffers. Any on-going transfers will not be flushed.
1.2.4.4.8 Preconditions
The SYS_CONSOLE_Initialize function should have been called before calling this function.
1.2.4.4.8 Parameters
| Parameters | Description |
|---|---|
| handle | Handle to the console instance |
1.2.4.4.8 Returns
True - If the operation is successful.
False - In case of failure.
1.2.4.4.8 Example
SYS_CONSOLE_HANDLE myConsoleHandle;
bool status;
// myConsoleHandle is assumed to be a valid console handle
status = SYS_CONSOLE_Flush(myConsoleHandle);
if (status == false)
{
// Handle error
}
1.2.4.4.8 Remarks
This API may do nothing and return true, where the read and write are not buffered.