1.2.4.4.12 SYS_CONSOLE_WriteCountGet Function
1.2.4.4.12 C
ssize_t SYS_CONSOLE_WriteCountGet(const SYS_CONSOLE_HANDLE handle)
1.2.4.4.12 Summary
Returns the number of bytes pending for transmission in the transmit buffer.
1.2.4.4.12 Description
This function indicates the number of bytes pending for transmission in the transmit buffer.
1.2.4.4.12 Preconditions
The SYS_CONSOLE_Initialize function should have been called before calling this function.
1.2.4.4.12 Parameters
| Parameters | Description |
|---|---|
| handle | Handle to the console instance |
1.2.4.4.12 Returns
The return value indicates the number of bytes present in the transmit buffer waiting to be transmitted. Returns -1 in case of any error.
1.2.4.4.12 Example
ssize_t nTxBytesPending; SYS_CONSOLE_HANDLE myConsoleHandle; nTxBytesPending = SYS_CONSOLE_WriteCountGet(myConsoleHandle); if (nTxBytesPending == -1) { // API reported error } if (nTxBytesPending == 0) { // All the data has been written to the console }
1.2.4.4.12 Remarks
None.