1.2.1.4 SYS_MEDIA_BLOCK_EVENT Enum
1.2.1.4 C
typedef enum
{
/* Block operation has been completed successfully. */
SYS_MEDIA_EVENT_BLOCK_COMMAND_COMPLETE,
/* There was an error during the block operation */
SYS_MEDIA_EVENT_BLOCK_COMMAND_ERROR
} SYS_MEDIA_BLOCK_EVENT;
1.2.1.4 Summary
Identifies the possible events that can result from a request.
1.2.1.4 Description
This enumeration identifies the possible events that can result from a media.
1.2.1.4 Remarks
One of these values is passed in the "event" parameter of the event handling callback function that client registered with the driver by setting the event handler when a block request is completed.