1.2.1.17 SYS_MODULE_INITIALIZE_ROUTINE Typedef

1.2.1.17 C

typedef SYS_MODULE_OBJ (* SYS_MODULE_INITIALIZE_ROUTINE) ( const SYS_MODULE_INDEX index,

1.2.1.17 Summary

Pointer to a routine that initializes a system module (driver, library, or system-maintained application).

1.2.1.17 Description

This data type is a pointer to a routine that initializes a system module (driver, library, or system-maintained application).

1.2.1.17 Precondition

The low-level board initialization must have (and will be) completed before the system will call the initialization routine for any modules.

1.2.1.17 Parameters

ParametersDescription
indexIdentifier for the module instance to be initialized.
initPointer to the data structure containing any data necessary to initialize the module. This pointer may be null if no data is required and default initialization is to be used.

1.2.1.17 Returns

A handle to the instance of the system module that was initialized. This handle is a necessary parameter to all of the other system-module level routines for that module.

1.2.1.17 Remarks

This function will only be called once during system initialization.