1.3.4.1.6 MAC_PLC_GetRequestSync Function
C
MAC_STATUS MAC_PLC_GetRequestSync
(
MAC_PLC_PIB_ATTRIBUTE attribute,
uint16_t index,
MAC_PIB_VALUE *pibValue
);
Summary
The MAC_PLC_GetRequestSync primitive gets the value of an attribute in the MAC PLC layer Parameter Information Base (PIB).
Description
GetRequestSync primitive is used to get the value of a PIB. Sync suffix indicates that result is provided upon function call return, in the pibValue parameter.
Precondition
MAC_PLC_Init routine must have been called before.
Parameters
| Param | Description |
|---|---|
| attribute | Identifier of the Attribute to retrieve value. See MAC_PLC_PIB_ATTRIBUTE. |
| index | Index of element in case Attribute is a table. Otherwise index must be set to '0'. |
| pibValue | Pointer to MAC_PIB_VALUE object where value will be returned. |
Returns
Result of get operation as a MAC_STATUS code.
Example
MAC_STATUS status;
MAC_PIB_VALUE value;
status = MAC_PLC_GetRequestSync(MAC_PIB_MAX_FRAME_RETRIES, 0, &value);
if (status == MAC_STATUS_SUCCESS)
{
// Get value from 'value' parameter
}
Remarks
None.